Unable to add motor from hardware catalog

Unable to add this B&R 8LSA4444db022D000-3 motor from hardware catalog in Automation Studio v4.12.13.127 SP#AS site license.I tried to download it from Upgrades, but it’s not getting installed. As after downloading installation window doesn’t come at all.

Hi @samikshaunhale21 ,

the UAC window may be ‘hidden’ somewhere.

you can try to download the installation exe manually

[8lsa44.db022d000-3]

and try a local Upgrade

I tried to do that,
It’s not working either.
What could be the issue ?

can you try this batch file ? (do not start AS)
Probably you have to adjust the AS installation path inside.

install.zip (269.7 KB)

Hi Samiksha,what is the status of your topic, can you update us with your solution?

you can close the case.i have find slution

and what is your solution? If you share it then others can benefit from it as well :slight_smile:

Manual installation was the solution.i have marked in the above feed.