Alex
(Alexandre Gallet)
1
Hello,
I want to use the “Servo loop optimizer” in AS6, but this feature is always greyed in the “Open” menu ….
When or from where I can use it ?
Hello,
The “Servo Loop Optimizer” in the Automation Studio is only supported with ACP10.
If MappMotion is used you can not use this integrated ServoLoopOptimizer directly.
Up to MappCockpit/MappMotion Version 6.3:
- Make a Trace manualy in MappCockpit
- Export Data
- Open a ACP10 AS-Projekt, Import Data and make the analysis there.
See this Guide:
From one of the next MappCockpit Version 6.x
it is planed to offer a Cockpit Implementation as a follow up of the Servo Loop Optimizer.
Greetings
Michael
kovarj
(Jaroslav Kovar)
3
I marked @michael.bertsch’s answer as a solution, but feel free @Alex to continue the discussion if needed.