Good evening,
I want to change the ip Adresses of my plc. In order to do it by using asarcfg is not the problem.
Is there any widged which i can use to get directly the ip Adress e.g. 10.10.10.5 complete with the dots and also formated to take it directly to the fubs or do i need to place a couple numeric input widgets in a row to show each of the four numbers of the adress.
Thanks
There is not a specific Mapp View widget or VC4 control that would handle this formatting automatically.
The general VC4 solution is to use a String Control with formatting checking upon completion, or 4 Numeric Controls again some focus control, and formatting upon completion.
For mapp View I think most would use Text Input widget, again with some formatting checking upon completion, though you may be able to do something with event handling but Iām not sure.
In theory you might be able to create a compound widget that does this functionality in a crude way, but if you are looking for a widget specifically for a IP4 address formatting, you probably need to look for using the mapp View 6.3 mapp Script, or the mapp View Widget development toolchain.
when i use the TextInput Widget for this issue. Is it possible - like in VC4 - to change the Keypad to a numeric Keypad so that only numbers and ā.ā are available?
B&R Online Help Custom keyboard help info