Simulate plc is different

The RUN PC is different with my configuration PLC :sob: :sob:

Hi Alex,
This mighe be because of 2 or more AS projects with simulation are open at the same time.
Please make sure that only one ARSim instance of the active project is open and then check.

I hope this will help you.

1 Like

HI,KAUSHAL

I’sure it just have one project, before it i have doubted for this situation and i closed all ,but it’s no change.

And i reconfiguration the PLC,but now it can’t connect.:sob:

Hi Alex,

In this case, i would suggest you to do following steps.

  1. Exit ARSim application ( right click on the ARSim icon and exit)

  2. Go to project → Project Installation → Offline Installation

thank you for you help,:grin:

Is your problem solved after a fresh ArSim reinstallation?