T50 - OPC UA method call

Hi,

I am using a Power PanelT50 and a PLC X20CP0484. I would like to activate the OPC UA server on the T50 and allow the PLC to adjust its brightness via a method call. I found a section in the T50 manual that explains how to adjust brightness using an OPC UA method call. However, since I am new to OPC UA, I am not familiar with the configuration or how to use the relevant libraries. I would appreciate it if you could guide me through the process.

See mappPanel sample on github:

Hi @ryechan2028

Did Corne’s link answer your question, or do you have additional questions for us?

This link requires a single sign on via an ABB account:

There is an issue with the GitHub and this is still under investigation.
The Archive should still work:
B&R Industrial Automation [Archive] · GitHub