- create a terminal project - see help
- install server (Offline Install or Transfer)
- create USB stick pro a client installation in AS
- navigate to Project → Project Installation → Generate Project Installation Package
- “Normal B&R module system (1 partition)” as the B&R module system must be chosen (otherwise installation won’t happen)
- insert USB stick to a panel and bring it to the BOOT mode
3 Likes
Hi,
Link is down. Do you think it can be reuploaded somehow?
Hi,
not 100% sure but I think it could have been this link:
1 Like