Panel 5MP050.0653-04 worked without any issues, but BR VNC Viewer had to be launched manually after powering on to control the equipment. For autorun, we created two text files in the \IPSM\ folder using the built-in WinCE5 text editor: START.TXT and START.DAT, each with the same content: ERRORMSG=1 TOUCHCAL=1 RUN=’’\Windows\Explorer.exe’’ RUN=’’\Windows\BrWinCEVNC.exe’’ 192.168.0.97:5900
We made no other changes to the system. As a result, after extracting from the image and starting WinCE5.0, the panel freezes—the gray screen shows no image, only a moving mouse cursor.
Is there any way to access the folder \IPSM\ from the outside and delete the files?
Since there are no other user files on the panel, is it possible to clear all user data or, for example, perform a “factory reset”? Maybe someone knows the purpose purpose of the RS232,USB and DIP SWITCHES under the back cover of Mobile panel MP 40/50?