Use of quick stop function for trigger1 and trigger2

Hello,
i’m using 8V1180.001-2 drive, want to use trigger1 and trigger2 inputs of the drive for quickstop function. i have tried (ncACTIV_LO + ncQUICKSTOP) option for both trigger inputs in the init parameter table but getting the error (1002 - Digital input: Quickstop enable bits/outside the valid rage). Also tried using the DIG_IN_QUICKSTOP_ENABLE ParaID but getting error.
How do i use trigger1 and trigger2 for quickstop functionality.

Hi,
you can use either trigger1 or trigger2 as Quickstop input but not both simultaneously.
Unfortunately the editor for ini file allows to set this wrong configuration :frowning:

Thank you for the reply.