Which programs or tasks need to use system task t3 and tNet0?

Which programs or tasks need to use system task t3 and tNet0?

Hi,

I have no idea for “t3” task, for “tNet0” it’s link to networking.

So there is no program it’s the runtime itself, at least for “tNet0” if it’s really link to networking.

Thanks a lot.
This problem is solved by resetting a function module with network reading files.

1 Like

Hi there, do you have any more details you could share about this function module? I am having a similar issue but can’t find the source.

Hello, this question was consulted by a colleague on behalf of a client. I helped analyze the situation.

Eventually, the client resolved the issue, claiming it was due to a network file reading program. It might be that this program only needs to be triggered once and then wait for the result, but it keeps triggering. This is all the information I know.

1 Like