Hi,
With the new X20DS838A module that supports 32 bytes input and output for every channel, I saw that the size of input/output was configured in steps of 4 bytes
Compared to X20DS438A that are in steps of 1 byte.
I have IO-Link devices that for example are using 7 bytes output and 18 bytes input. How will that work with the new module? Are the device I want to communicate with skipping the addtional bytes that are configured in AS?