X20EDS410 web interface not accessible

Hello,

After following the commisioning guide for X20EDS410, I’ve set up the unit according to our application needs. I’ve made an image of it, and flashed a new unit with this image. With the new unit I can’t access the web interface, and I also have issues with DNS (looks like systemd-resolved issues?). I can access it via SSH and everything else looks fine, only DNS and web interface seems to be missing. I’ve since managed to get around the DNS issues, but when I try to access the web interface at the device IP on port 8080, I’m greeted with a Internal Server Error. Is there any way to see the logs from the application that’s running the web server?

Is there a better way to commission new units with our application software on it rather than what I described above? Anyone else bumped into similar issues? Grateful for any help or advise.

Emil

Hi @j.lagarde, obviously no one from the Community can help you with your topic, so please get in touch with your local support office. Please update us with your findings. Thanks a lot, Jaroslav

It looks like the issue is because of manually applied updates via apt-get

hi @Emil_Hjelm thanks for update :slight_smile: