Hi, is it possible to use a X20IF2772 to communicate via the CAN_Lib and the CMS protocol like you would with an X20CS1070?
short answer: yes, sure.
longer answer:
actually the question is the wrong way around
.
X20IF2772 always works with the CAN_Lib, X20CS… only under certain conditions (ability to use a ‘stream’ model).
thanks, sorry for the basic question I’ve just started to use B&R systems.
I have used an X20IF2772 only with the AsCANopen Lib and everything was very simple to setup via the card configuration and I/O mapping. What should I do on the card configuration in this case?
What should I do on the card configuration in this case?
you should deactivate the CANopen master and the CANIO functionality.