I wonder how to set the node id outside of the limited address provide in the manual.
Ex if i want to set the node 40…
Hi Tommy,
The only node numbers that can be used are the ones in that table. It is not possible to set the bus controller’s Node ID to any other value.
Some uninvited additional information.
The only way to set the node ID is with a resistor. No LSS. etc🤣