-1070584537 - Facing error while project installation via LAN

Greetings,

We’ve received a report from one of our customers indicating an error during project installation via LAN. Here are the observations:

Hardware: 4PPC80

  1. Project installation via USB is successful.
  2. An error is being indicated when the AR status shows as N/A.
  3. When the AR status is N/A, the error persists during project installation via LAN in Stop Mode.
  4. Similarly, in Service Mode, when the AR status is N/A, the error occurs during project installation via LAN.

What steps can be taken to resolve this issue for customers who wish to install the project via LAN when the AR status is N/A?










It seems that there is no USER partition (F:).
What size is defined at the Minimum user partition size ?

It is defined as 300MiB

As far as I know on a hypervisor system, a new partitioning can only be forced by reinstalling the entire system using a USB installation stick. Therefore, the size of a user partition cannot be changed on a hypervisor system without reinstalling the entire system.

Hello @ravi.shah,

It looks like you got some good answers from Corne and Jaroslav, and it has been a couple of weeks since the last activity on this post. If the answers helped you with your question, can you help the next person with the same question by marking the solution on the information which helped you the most? If you still have open questions on this topic, can you provide an update?

Thank you.

how can i reinstall the entire system using a USB installation stick? i’m facing the same problem but i’m already creating an usb install drive with the “create USB install drive” command but i still get the AR status N/A message. Thank you

This is basically correct, to be sure that problem is not your project related, please create empty project only with hw configuration using C80, then generate USB install drive and boot from it.

I tried it with an empty project and it works. What could it depend on? Thank you

this topic is closed. Please continue in another one you have already created.