About ACOPOSmulti current

Dear,
I want to get the input and output current values of acoposmulti-8bvp module, which ID number can be read?
In addition, I found an ID1154: Power stage: Rectifier: Current in AS-help. But when I read it, the values are all 0. How to use it?

Hi,
In principle, the 8BVP is similar to 8BVI. In this case, the ‘motor’ is the mains.
This means that 214 (ICTRL_ISQ_ACT) and 219 (ICTRL_ISD_ACT) are used here for the input currents.

Hi,
Thank you for your reply.
I would like to confirm again whether the ID214 and ID219 is AC380v L1/L2/L3 input to 8BVP or 8BVP input to DCBUS?

Hi,
yes, they are on primary side. On DC Bus there is no current sensor.