ACOPOS Micro SSI Elektronisches Typenschild auslesen

Hallo,

ist der ACOPOS Micro SSI in der Lage das elektronische Typenschild eines Motors über das SSI Interface zu lesen? Wenn ja wann genau findet dieser Vorgang statt?

Beste Grüße
Dominik

Hi,

Is the ACOPOS Micro SSI able to read the electronic nameplate of a motor via the SSI interface? If so, when exactly does this process take place?

you mean 80SD100XD.C033-01 ?

no. However, there is a way to identify known motors via the current rise:

Motor identification

No sorry, I mean the 80VD100PS.C03X-01 for Servo Motors. I hoped that it would be as easy as with EnDat2.0. But thanks for the information :slightly_smiling_face:

ok. But the answer is similar.

SSI is just a simple shift register with no space for transfering anything else but the position data.

Even with Endat motors it is only possible if the encoder memory has been written in a way that is compatible with ACOPOS.

Best Regards,