Hi all,
I’m Donato from Merck Serono, I have some issues with APC 910 PXE boot from ethernet.
-BIOS version APCCR117 (08/23/2019)
I’ve enabled the UEFI eth boot from bios but but when I start the PC it remains in no boot option.
I’ve tried to change some configuration, in order to enable the the ethernet device for boot:
-Network Stack driver support: enabled
-UEFI fast boot: Enabled/Disabled (both configuration)
-Boot priority selection: Type based
with:
1st: onboard LAN
2st: external LAN
if I connect a different PC (thinclient) into same eth port the PXE boot start well so I don’t have network issue.
I can share more information or screenshots if it might be helpful.
some one have any idea how I can solve?
Thanks in advance