APROL Multiple CC operator accounts on the same runtime PC

Good Afternoon,

In APROL, Is it possible to have multiple CC operator accounts on a runtime PC?

I require separate accounts for four T50 screens that all VNC into a runtime PC. The four T50 screens would have their own accounts allowing each screen to show different data
depending on the CC account. In this example only certain on call engineers would get the data.

I have attempted this but unable to connect to the APROL loader and download to the new operator account.

If anyone has any ideas on this solution it would be greatly appreciated.

Dale Webb

Hello Dale,
Yes, you can configure four operator accounts on one operator station.

If you use APROL R4.4 you should be able to download the new accounts first with the option “only download aprolloader configuration” and after that “all”.

BR, Christian