AS6.5 – New CFast/CFexpress cards not detected during offline installation

Hi everyone,

We are experiencing an issue with Automation Studio 6.5 when performing an offline installation on new, uninitialized memory cards.

When trying to perform an offline installation with AS6.5, the memory card is not detected/listed as an available disk, making it impossible to proceed with the installation.
However, the exact same memory card, PC, and card reader work perfectly fine with AS4.12.

Even more interesting:
Once the memory card has been initialized using AS4.12, it is also recognized by AS6.5, and offline installation works as expected.

The issue is reproducible with different memory cards and card readers (both CFast and CFexpress).

What I’ve found out so far

  • Windows detects the physical disk, even though it does not appear in Windows Explorer, Just like a brand new SSD/HDD would.

  • New memory cards do not have a partition table (recognized by Windows). This can be verified using PowerShell’s Get-Disk command, which reports PartitionStyle = RAW.

  • If the memory card is initialized using Windows Disk Management (diskmgmt.msc), meaning a partition table is created, AS6.5 recognizes it and offline installation works.
    Unfortunately, initializing a disk using Windows Disk Management requires administrator privileges, which we do not have on our company laptops.

My suspicion: B&R Disk Image service?

We have experienced issues with the B&R Disk Image service in the past, so I suspect that it might be involved again.
Both services are installed and running on the same PC:

AS4.12 – B&R Disk Image
  • Service name: BrDiskImageSvcx
  • Executable: C:\Program Files\BRAutomation4\PVI\V4.12\PVI\Tools\PVITransfer\BrDiskImageSvc.exe
AS6.5 – B&R Disk Image 6
  • Service name: BrDiskImage6Svcx
  • Executable: C:\Program Files (x86)\BRAutomation\PVI6\PVI\Tools\PVITransfer\BrDiskImageSvc.exe

Both services are configured to start automatically and run under LocalSystem.

My suspicion is that AS6.5 might handle the initial disk initialization differently from AS4.12, or that there might be an issue with the newer Disk Image service.




Has anyone experienced something similar?

Is this a known issue with AS6.5, or does anyone have an idea what could be causing it?

In particular, is there any difference in how AS4.12 and AS6.5 handle uninitialized (RAW) disks during offline installation?

Any hints or suggestions would be greatly appreciated!

Thanks in advance!

Hi @PatrickS,

as far as I know, you’re completely right - the Disk Image Service of ASW6 needs a pre-initialized CF / CFast / CFast Express to use the card (or, as I understood it: a mapped drive letter to the card in Windows).

I’m personally not aware what’s the reason behind (but I could imagine it’s a combination of cyber security measures + avoiding elevated rights when using RUC).
Unfortunately, I also don’t know if this changes in future - if my assumption about the reason behind is true, then sure not.

But, afaik, at least in past normally storage cards were delivered from B&R with a default partition setup, not as RAW system (exactly for compatibility reasons).
To check if there is / was a change in that delivery strategy, or if there has been some temporary issue in production / delivery, can you please reach out to your local support with a reference to this post + the CFastExpress serial number(s) so that we can check if there’s a supply chain topic behind?

Best regards, Alex!

PS, just as 2nd reference:

Is an usb installation working? (keyboard, sceen needed)
For all APC/PPC this usb installation is possible, without using a card reader.

I opened a ticket regarding this behaviour (drives for offline installation need to be initialized by Windows before AS6 detects them) in August 2025. I asked about the current state in October 2025 and the local B&R support answered my question: “The ticket is with our development team [in austria]. I have asked them for an update on its current status.”
The ticket was closed without any answer from Austria in July 2026. :woman_shrugging:

@alexander.hefner:
Sounds very plausible, thank you.
I will try to get some serial numbers and open a support ticket.

@corne.geerts:
I honestly didn’t try, as this hasn’t been our workflow in the past. We also deactivate the USB install functionality on our PLCs.
But I may give this a try (may take a few days).

@Bjorn_Kanter:
Did you get a CASE-number for this issue?
It may be helpfull to reference it, when our local (german) B&R office reaches out to the HQ.

I will try to get some more information about this issue and keep you updated.

Thanks everyone for your help!

Hi @PatrickS,

I already got the number from @Bjorn_Kanter, and as I already assumed it was a CSP not a CASE which at least maybe explain the “automatic closing” … I’ll check and if I find out more I’ll share it here.

BG Alex

This is a bootable USB stick and not dependent on project settings.

if I can help you Alex anyhow, let me know.

Just to share some light here…

The issue will be fixed with AS6.9 / PVI 6.9

It was no cyber security issue or similar. Basically AS could not deal with large CFExpress cards and therefor the so called “diskmanagement” got reworked. As a drawback it could no longer deal with unpartitioned CF cards

This is now fixed and AS6.9 should also accept such cards

best regards

Oliver

We don’t have any display outputs on our PLCs, so only solutions without any interaction required are feasable.
But I tried the USB install method anyways. With the limitation of not beeing able to boot to another device the results are:

On an already commissioned PLC, this didn’t work.
That is what I was expecting as we deactivated the USB install setting already several months / years ago (seems to be the default setting for AS6 now).

On the other hand it works like a charm with an empty one.
As I said: I didn’t consider this solution, as we never used USB installation.

But we will use this method as a temporary solution for the time being (or until AS/PVI 6.9 is released).

Thank you @oliver_D for the insights :+1:

@PatrickS,

Apologizes!
As I now know, the information that memory cards are delivered pre-formatted was outdated.
This has changed somewhen in past (I don’t know the exact point in time) due to the different use-cases and scenarios how the cards are used (AR or GPOS or HV or …).

So there wasn’t a delivery issue but a changed process I were not aware of…
… as already mentioned by Oliver, an update in ASW 6.9 will also make the usage of unformatted cards with RUC available.

Best regards, Alex