Offline installation on CFast for APC2200

Hi everyone!

For some reason, I am unable to do an offline installation on a CFast.

I am using a dedicated industrial computer with one integrated CFast reader. This computer has a clean Windows install and a fresh Automation Studio (AS 4.8.7.28) install. After enabling the reader from BIOS, the CFast appears on Windows, and I am able to create, edit, and delete partitions on it, but Automation Studio does not detect the CFast as a CFast…

At the moment, I have tried to:

  • Verify BIOS settings, nothing apart from enabling the peripheral and the hot plug
  • Run AS as Administrator
  • Remove all partitions on CFast
  • Create a new partition on CFast
  • Upgrade PVI to version 4.8.6.11

Any idea on what can cause the issue or what to look for?

Let me know if you need more specific information to help me.

Hello,

Which version of Windows do you use? Be aware of the AS - Windows version compatibility.

Hello Pavel

I am using Windows 10 Enterprise LTSC (ver 1809)

Is this device detected as “removeable” device ?

As far as I remember AS cannot access “harddrives” do to the fact that you could overwrited fixed built in drives. I would say this could be your issue and you could test this if you use a USB adapter. If it then works we kjnow it is an issue with the “fixed” drive

Hi Oliver,
I have tested with a USB card reader, and it works. As you said, the issue is probably connected to the fact that AS detects the CFast reader integrated into the PC as a hard drive.
Is there a way to change this? BIOS or Windows parameter?

As far as I know this is not possible due to the fact that Windows relies on the controller of this device

The controller on the mainboard then tells Windows that this is a built in drive (and not a USB stick

I have dug a bit into the BIOS settings.

As you can see, the ATA port 3 is set as “Hot Plug” (as a removable device should be).

At this point, I think it is a Windows issue where it misinterprets BIOS information. At the moment, the only workaround is to use an external CFast card reader.

I will leave the thread open for a bit to see if anyone knows a fix for this; otherwise, an external reader is the only solution.

I don’t think that “hotplug” means it is handled as a removeable device like a USB stick

As I am quite unsure about this I asked Copilot about this and here is its response:

(I know that AI like Copilot and others are not always correct but the answer seems reasonable)