Dear engineers, I’m having a major issue and would appreciate your help. Recently, after repairing a device, it has failed to start up.
As shown in the following picture, there is an error.
Subsequently, after I performed the reinstallation, although the software could connect normally (with the interface showing green), it still reported a network failure.
Then I attempted to restore the files in AR010. Although the network was stable, there were still other errors occurring.
The content of the AR010log.txt file:
Tue Mar 27 07:08:07 2012
RTOS-Driver COM1 : RTOS Serial port
RTOS-Driver COM2 : RTOS Serial port
Number of processors :1 active core(s):0x1
Cores in boot.ini : /numproc=1
Bernecker & Rainer
IP shared Windows: 10.100.4.115
IP shared AR: 10.100.4.116
Timeout = 0[sec]
Retrycount = 30
Tue Mar 27 07:08:08 2012
Dongle for ARwin found!
Dongle for NC found!
BIOS-Version : 1.19
BIOS-Type : H
COMMAND_COLDSTART
Product: VxWin V5.0.00 (5.0.0.39)
Base: V5.0.0.39
RtosWin version: 5.0
Hosting OS: Windows XP Embedded Service Pack 3.0 (32 bit)
UploadRTOS.dll version: 7.18.18.0
RtosDrv - Realtime OS Driver
Driver version 9.1.10.0
Inf file version 1.2.4.0
Installer version 0.0.0.1
Required VMF version 1.27.11.0
RtosVnet - Realtime OS Virtual Network Adapter
Driver version 7.7.0.0
Inf file version 1.1.3.0
Installer version 0.0.0.1
Required VMF version 1.20.0.0
RteDevice - RTOS Serial port (COM1)
Driver version 5.3.3.0
Inf file version 1.4.2.0
Installer version 1.0.5.0
Required VMF version 1.26.0.0
RteDevice - RTOS Serial port (COM2)
Driver version 5.3.3.0
Inf file version 1.4.2.0
Installer version 1.0.4.0
Required VMF version 1.26.0.0
RteDevice - B&R Interface Card for ARwin
Driver version 5.3.3.0
Inf file version 1.4.2.0
Installer version 1.0.5.0
Required VMF version 1.26.0.0
RteDevice - B&R Interface Card for ARwin #9
Driver version 5.3.3.0
Inf file version 1.4.2.0
Installer version 1.0.5.0
Required VMF version 1.26.0.0
RteDevice - B&R Interface Card for ARwin #10
Driver version 5.3.3.0
Inf file version 1.4.2.0
Installer version 1.0.5.0
Required VMF version 1.26.0.0
RteDevice - B&R Interface Card for ARwin #11
Driver version 5.3.3.0
Inf file version 1.4.2.0
Installer version 1.0.5.0
Required VMF version 1.26.0.0
RteDevice - B&R Interface Card for ARwin #16
Driver version 5.3.3.0
Inf file version 1.4.2.0
Installer version 1.0.5.0
Required VMF version 1.26.0.0
RteDevice - B&R Interface Card for ARwin #17
Driver version 5.3.3.0
Inf file version 1.4.2.0
Installer version 1.0.5.0
Required VMF version 1.26.0.0
RteDevice - B&R Interface Card for ARwin #18
Driver version 5.3.3.0
Inf file version 1.4.2.0
Installer version 1.0.5.0
Required VMF version 1.26.0.0
RteDevice - B&R Interface Card for ARwin #19
Driver version 5.3.3.0
Inf file version 1.4.2.0
Installer version 1.0.5.0
Required VMF version 1.26.0.0
RteDevice - Realtime OS Virtual Network Adapter
Driver version ignored
Inf file version ignored
Installer version ignored
Required VMF version 1.20.0.0
RteDevice - Realtime OS Driver
Driver version ignored
Inf file version ignored
Installer version ignored
Required VMF version 1.27.11.0
RtosService version: 3.5.4.0
RtosControl version: 7.6.4.2
Virtual machine framework version: 1.27.12.0
Virtual machine framework version required by Uploader: 1.27.11.0
Reservation active : base 64Mb and size 200000Kb.
Loading VMF...Ok
Virtual machine framework version required by OS: 1.27.x.x
Start OS - Id:0... Ok
Waiting for Windows <--> Realtime OS communication subsystems...... ok
AR-version : P4.02
Unloading VMF...Ok
Product: VxWin V5.0.00 (5.0.0.39)
Base: V5.0.0.39
RtosWin version: 5.0
Hosting OS: Windows XP Embedded Service Pack 3.0 (32 bit)
UploadRTOS.dll version: 7.18.18.0
RtosDrv - Realtime OS Driver
Driver version 9.1.10.0
Inf file version 1.2.4.0
Installer version 0.0.0.1
Required VMF version 1.27.11.0
RtosVnet - Realtime OS Virtual Network Adapter
Driver version 7.7.0.0
Inf file version 1.1.3.0
Installer version 0.0.0.1
Required VMF version 1.20.0.0
RteDevice - RTOS Serial port (COM1)
Driver version 5.3.3.0
Inf file version 1.4.2.0
Installer version 1.0.5.0
Required VMF version 1.26.0.0
RteDevice - RTOS Serial port (COM2)
Driver version 5.3.3.0
Inf file version 1.4.2.0
Installer version 1.0.4.0
Required VMF version 1.26.0.0
RteDevice - B&R Interface Card for ARwin
Driver version 5.3.3.0
Inf file version 1.4.2.0
Installer version 1.0.5.0
Required VMF version 1.26.0.0
RteDevice - B&R Interface Card for ARwin #9
Driver version 5.3.3.0
Inf file version 1.4.2.0
Installer version 1.0.5.0
Required VMF version 1.26.0.0
RteDevice - B&R Interface Card for ARwin #10
Driver version 5.3.3.0
Inf file version 1.4.2.0
Installer version 1.0.5.0
Required VMF version 1.26.0.0
RteDevice - B&R Interface Card for ARwin #11
Driver version 5.3.3.0
Inf file version 1.4.2.0
Installer version 1.0.5.0
Required VMF version 1.26.0.0
RteDevice - B&R Interface Card for ARwin #16
Driver version 5.3.3.0
Inf file version 1.4.2.0
Installer version 1.0.5.0
Required VMF version 1.26.0.0
RteDevice - B&R Interface Card for ARwin #17
Driver version 5.3.3.0
Inf file version 1.4.2.0
Installer version 1.0.5.0
Required VMF version 1.26.0.0
RteDevice - B&R Interface Card for ARwin #18
Driver version 5.3.3.0
Inf file version 1.4.2.0
Installer version 1.0.5.0
Required VMF version 1.26.0.0
RteDevice - B&R Interface Card for ARwin #19
Driver version 5.3.3.0
Inf file version 1.4.2.0
Installer version 1.0.5.0
Required VMF version 1.26.0.0
RteDevice - Realtime OS Virtual Network Adapter
Driver version ignored
Inf file version ignored
Installer version ignored
Required VMF version 1.20.0.0
RteDevice - Realtime OS Driver
Driver version ignored
Inf file version ignored
Installer version ignored
Required VMF version 1.27.11.0
RtosService version: 3.5.4.0
RtosControl version: 7.6.4.2
Virtual machine framework version: 1.27.12.0
Virtual machine framework version required by Uploader: 1.27.11.0
Reservation active : base 64Mb and size 200000Kb.
Loading VMF...Ok
Virtual machine framework version required by OS: 1.27.x.x
Start OS - Id:0... Ok
Waiting for Windows <--> Realtime OS communication subsystems...... ok
AR-version : P4.02
ARwin Startup Console Log:
2012-03-27 07:24:23 $arlogsys:ERROR 26456, lpBin=0x0a738a94, ARLOG_LEVEL_WARNING, "ROOT", "DP: '$root:TemperatureCPU'"
2012-03-27 07:24:23 $arlogsys:ERROR 26456, lpBin=0x0a738a94, ARLOG_LEVEL_WARNING, "ROOT", "DP: '$root:SystemTime'"
2012-03-27 07:24:23 $arlogsys:ERROR 28713, lpBin=0x0a7388e4, ARLOG_LEVEL_WARNING, "ROOT", "Platformclass not found"
2012-03-27 07:24:19 $arlogsys:ERROR 28724, lpBin=0x0a738a64, ARLOG_LEVEL_WARNING, "ROOT", "vcpf010"
2012-03-27 07:24:19 $arlogsys:ERROR 28729, lpBin=0x0a738a14, ARLOG_LEVEL_WARNING, "ROOT", "HW-Platform not supported"
2012-03-27 07:24:19 $arlogsys:ERROR 28729, lpBin=0x0a738a04, ARLOG_LEVEL_WARNING, "ROOT", "HW-Platform not supported"
2012-03-27 07:23:49 $safety:ERROR 110403, lpBin=0x0c16178e, ARLOG_LEVEL_INFO, "DdxxIoSafetyLogger", "SL2.IF2.ST2.IF1.ST16: Info0=0x0000, Info1=0x00000000 "
2012-03-27 07:23:49 $safety:ERROR 110403, lpBin=0x0c161775, ARLOG_LEVEL_INFO, "DdxxIoSafetyLogger", "SL2.IF2.ST2.IF1.ST15: Info0=0x0000, Info1=0x00000000 "
2012-03-27 07:23:49 $safety:ERROR 110403, lpBin=0x0c161775, ARLOG_LEVEL_INFO, "DdxxIoSafetyLogger", "SL2.IF2.ST2.IF1.ST14: Info0=0x0000, Info1=0x00000000 "
2012-03-27 07:23:49 $safety:ERROR 110403, lpBin=0x0c1617a7, ARLOG_LEVEL_INFO, "DdxxIoSafetyLogger", "SL2.IF2.ST2.IF1.ST17: Info0=0x0000, Info1=0x00000000 "
2012-03-27 07:23:49 $safety:ERROR 110403, lpBin=0x0c16178e, ARLOG_LEVEL_INFO, "DdxxIoSafetyLogger", "SL2.IF2.ST2.IF1.ST12: Info0=0x0000, Info1=0x00000000 "
2012-03-27 07:23:49 $safety:ERROR 110403, lpBin=0x0c161775, ARLOG_LEVEL_INFO, "DdxxIoSafetyLogger", "SL2.IF2.ST2.IF1.ST11: Info0=0x0000, Info1=0x00000000 "
2012-03-27 07:23:49 $safety:ERROR 110403, lpBin=0x0c161775, ARLOG_LEVEL_INFO, "DdxxIoSafetyLogger", "SL2.IF2.ST2.IF1.ST13: Info0=0x0000, Info1=0x00000000 "
2012-03-27 07:23:46 $fieldbus:ERROR 0, lpBin=0x0c1af844, ARLOG_LEVEL_INFO, "DdxxIoProfiBus.SL1.IF2.ACC", "PROFIBUS Master parameter set"
2012-03-27 07:23:46 $fieldbus:ERROR 0, lpBin=0x0c1b00bf, ARLOG_LEVEL_INFO, "DdxxIoProfiBus.SL1.IF2.ACC", "PROFIBUS Slave 34 parameter set"
2012-03-27 07:23:46 $fieldbus:ERROR 0, lpBin=0x0c1b00bf, ARLOG_LEVEL_INFO, "DdxxIoProfiBus.SL1.IF2.ACC", "PROFIBUS Slave 33 parameter set"
2012-03-27 07:23:46 $fieldbus:ERROR 0, lpBin=0x0c1b00bf, ARLOG_LEVEL_INFO, "DdxxIoProfiBus.SL1.IF2.ACC", "PROFIBUS Slave 28 parameter set"
2012-03-27 07:23:46 $fieldbus:ERROR 0, lpBin=0x0c1b00bf, ARLOG_LEVEL_INFO, "DdxxIoProfiBus.SL1.IF2.ACC", "PROFIBUS Slave 27 parameter set"
2012-03-27 07:23:46 $fieldbus:ERROR 0, lpBin=0x0c1b00bf, ARLOG_LEVEL_INFO, "DdxxIoProfiBus.SL1.IF2.ACC", "PROFIBUS Slave 26 parameter set"
2012-03-27 07:23:46 $fieldbus:ERROR 0, lpBin=0x0c1b00bf, ARLOG_LEVEL_INFO, "DdxxIoProfiBus.SL1.IF2.ACC", "PROFIBUS Slave 25 parameter set"
2012-03-27 07:23:46 $fieldbus:ERROR 0, lpBin=0x0c1b00bf, ARLOG_LEVEL_INFO, "DdxxIoProfiBus.SL1.IF2.ACC", "PROFIBUS Slave 24 parameter set"
2012-03-27 07:23:46 $fieldbus:ERROR 0, lpBin=0x0c1b00bf, ARLOG_LEVEL_INFO, "DdxxIoProfiBus.SL1.IF2.ACC", "PROFIBUS Slave 23 parameter set"
2012-03-27 07:23:46 $fieldbus:ERROR 0, lpBin=0x0c1b00bf, ARLOG_LEVEL_INFO, "DdxxIoProfiBus.SL1.IF2.ACC", "PROFIBUS Slave 22 parameter set"
2012-03-27 07:23:46 $fieldbus:ERROR 0, lpBin=0x0c1b00bf, ARLOG_LEVEL_INFO, "DdxxIoProfiBus.SL1.IF2.ACC", "PROFIBUS Slave 21 parameter set"
2012-03-27 07:23:46 $fieldbus:ERROR 0, lpBin=0x0c1b00bf, ARLOG_LEVEL_INFO, "DdxxIoProfiBus.SL1.IF2.ACC", "PROFIBUS Slave 4 parameter set"
2012-03-27 07:23:44 $fieldbus:ERROR 0, lpBin=0x0c1b00bf, ARLOG_LEVEL_INFO, "DdxxIoProfiBus.SL1.IF2.ACC", "PROFIBUS Slave 3 parameter set"
2012-03-27 07:23:44 $fieldbus:ERROR 0, lpBin=0x00000000, ARLOG_LEVEL_INFO, "DdxxIoProfiBus.SL1.IF2.ACC", "Deleted static PROFIBUS configuration!"
2012-03-27 07:23:36 $safety:ERROR 114825, lpBin=0x0c161162, ARLOG_LEVEL_WARNING, "DdxxIoSafetyLogger", "SL2.IF2.ST1: SafeMODULE ID=12, Info1=0, Info2=0x0000 "
2012-03-27 07:23:36 $safety:ERROR 114825, lpBin=0x0c161162, ARLOG_LEVEL_WARNING, "DdxxIoSafetyLogger", "SL2.IF2.ST1: SafeMODULE ID=16, Info1=0, Info2=0x0000 "
2012-03-27 07:23:36 $safety:ERROR 114825, lpBin=0x0c161162, ARLOG_LEVEL_WARNING, "DdxxIoSafetyLogger", "SL2.IF2.ST1: SafeMODULE ID=15, Info1=0, Info2=0x0000 "
2012-03-27 07:23:36 $safety:ERROR 114825, lpBin=0x0c161162, ARLOG_LEVEL_WARNING, "DdxxIoSafetyLogger", "SL2.IF2.ST1: SafeMODULE ID=14, Info1=0, Info2=0x0000 "
2012-03-27 07:23:36 $safety:ERROR 114825, lpBin=0x0c161162, ARLOG_LEVEL_WARNING, "DdxxIoSafetyLogger", "SL2.IF2.ST1: SafeMODULE ID=11, Info1=0, Info2=0x0000 "
2012-03-27 07:23:36 $safety:ERROR 114825, lpBin=0x0c161162, ARLOG_LEVEL_WARNING, "DdxxIoSafetyLogger", "SL2.IF2.ST1: SafeMODULE ID=10, Info1=0, Info2=0x0000 "
2012-03-27 07:23:36 $safety:ERROR 114825, lpBin=0x0c161162, ARLOG_LEVEL_WARNING, "DdxxIoSafetyLogger", "SL2.IF2.ST1: SafeMODULE ID=13, Info1=0, Info2=0x0000 "
2012-03-27 07:23:35 $fieldbus:ERROR 0, lpBin=0x00000000, ARLOG_LEVEL_INFO, "DdxxIoProfiBus.SL1.IF2.ACC", "Static PROFIBUS configuration found!"
2012-03-27 07:23:35 $fieldbus:ERROR 0, lpBin=0x00000000, ARLOG_LEVEL_INFO, "DdxxIoProfiBus.SL1.IF2.ACC", "Fieldbus interface: DPM BRIE - Version: V01.201 04.07.05 (Version V01.097 or higher is supported!)"
2012-03-27 07:23:35 $fieldbus:ERROR 0, lpBin=0x00000000, ARLOG_LEVEL_INFO, "DdxxIoProfiBus.SL1.IF2.ACC", "Startup PROFIBUS driver"
2012-03-27 07:23:34 $arlogsys:ERROR 28729, lpBin=0x0a7389d4, ARLOG_LEVEL_WARNING, "ROOT", "HW-Platform not supported"
2012-03-27 07:23:33 $arlogsys:ERROR 9212, lpBin=0x0a738ea4, ARLOG_LEVEL_WARNING, "ROOT", "Boot"
2012-03-27 07:23:32 $arlogsys:ERROR 30964, lpBin=0x0a738d24, ARLOG_LEVEL_FATAL, "ROOT", "ArConfig: CPU mismatch"
2012-03-27 07:23:31 $arlogsys:ERROR 0, lpBin=0x0a738cb4, ARLOG_LEVEL_WARNING, "ROOT", "missing descr. in HWD <0xa3ed>"
I hope everyone can help figure out the solution. Thank you very much.