Automation studio v2.01 or v2.38

Hi Dears

I need Automation Studio v2.01, please help me, I would like to reload a program to cp476

project file name is * .prj

thank you for attention _my email is sharif110@gmail.com

for example one file contain pc4.prj

PG Version : V 2.38
GDM-Objektliste : erstellt am 05.10.1998

³ Nr. ³ Taskname ³ RPS ³Prozessor ³Typ ³TC # ³Init-Typ³
ÃÄÄÄÄÄÅÄÄÄÄÄÄÄÄÄÄÄÄÅÄÄÄÄÄÄÄÄÄÄÅÄÄÄÄÄÄÄÄÄÄÅÄÄÄÄÄÄÄÅÄÄÄÄÄÄÅÄÄÄÄÄÄÄÄ´
³ 7 ³ bed_tab ³ MAIN_PLC ³ CP_476 ³ DAT ³ - ³ ³
³ 8 ³ tv_mov ³ MAIN_PLC ³ CP_476 ³ DAT ³ - ³ ³
³ 9 ³ a_mov_nr ³ MAIN_PLC ³ CP_476 ³ DAT ³ - ³ ³
³ 10 ³ param ³ MAIN_PLC ³ CP_476 ³ DAT ³ - ³ ³
³ 11 ³ z_param ³ MAIN_PLC ³ CP_476 ³ DAT ³ - ³ ³
³ 12 ³ can_dat ³ MAIN_PLC ³ CP_476 ³ DAT ³ - ³ ³
³ 13 ³ io_check ³ MAIN_PLC ³ CP_476 ³ SRC ³ 22 ³ SRC ³
³ 14 ³ option_1 ³ MAIN_PLC ³ CP_476 ³ SRC ³ 1 ³ SRC ³
³ 15 ³ waymes ³ MAIN_PLC ³ CP_476 ³ SRC ³ 1 ³ SRC ³
³ 16 ³ out_clr ³ MAIN_PLC ³ CP_476 ³ SRC ³ 1 ³ ³
³ 17 ³ hand ³ MAIN_PLC ³ CP_476 ³ SRC ³ 1 ³ SRC ³
³ 18 ³ m_contrl ³ MAIN_PLC ³ CP_476 ³ SRC ³ 1 ³ ³
³ 19 ³ m_ctrl_1 ³ MAIN_PLC ³ CP_476 ³ SRC ³ 1 ³ ³
³ 20 ³ auto ³ MAIN_PLC ³ CP_476 ³ SRC ³ 1 ³ SRC ³
³ 21 ³ startpos ³ MAIN_PLC ³ CP_476 ³ SRC ³ 1 ³ ³
³ 22 ³ config ³ MAIN_PLC ³ CP_476 ³ SRC ³ 1 ³ SRC ³
³ 23 ³ modectrl ³ MAIN_PLC ³ CP_476 ³ SRC ³ 2 ³ SRC ³
³ 24 ³ alarm ³ MAIN_PLC ³ CP_476 ³ SRC ³ 2 ³ SRC ³
³ 25 ³ times ³ MAIN_PLC ³ CP_476 ³ SRC ³ 2 ³ ³
³ 26 ³ t_out1 ³ MAIN_PLC ³ CP_476 ³ SRC ³ 2 ³ ³
³ 27 ³ spc_esk ³ MAIN_PLC ³ CP_476 ³ SRC ³ 2 ³ SRC ³
³ 28 ³ tests ³ MAIN_PLC ³ CP_476 ³ SRC ³ 3 ³ ³
³ 29 ³ motor ³ MAIN_PLC ³ CP_476 ³ SRC ³ 3 ³ ³
³ 30 ³ regler ³ MAIN_PLC ³ CP_476 ³ SRC ³ 3 ³ SRC ³
³ 31 ³ m_contr2 ³ MAIN_PLC ³ CP_476 ³ SRC ³ 3 ³ ³
³ 32 ³ seri_com ³ MAIN_PLC ³ CP_476 ³ SRC ³ 3 ³ SRC ³
³ 33 ³ pmc ³ MAIN_PLC ³ CP_476 ³ SRC ³ 3 ³ ³
³ 34 ³ protocol ³ MAIN_PLC ³ CP_476 ³ SRC ³ 3 ³ SRC ³
³ 35 ³ mapl_4pl ³ MAIN_PLC ³ CP_476 ³ SRC ³ 3 ³ SRC ³
³ 36 ³ lim_set ³ MAIN_PLC ³ CP_476 ³ SRC ³ 4 ³ SRC ³
³ 37 ³ bit_byte ³ MAIN_PLC ³ CP_476 ³ SRC ³ 4 ³ SRC ³
³ 38 ³ calculat ³ MAIN_PLC ³ CP_476 ³ SRC ³ 4 ³ SRC ³
³ 39 ³ cycl_con ³ MAIN_PLC ³ CP_476 ³ SRC ³ 4 ³ ³
³ 40 ³ clock ³ MAIN_PLC ³ CP_476 ³ SRC ³ 4 ³ ³
³ 41 ³ pid_opt ³ MAIN_PLC ³ CP_476 ³ SRC ³ 4 ³ SRC ³
³ 42 ³ can_20a ³ MAIN_PLC ³ CP_476 ³ SRC ³ 4 ³ SRC ³
³ 43 ³ userpage ³ MAIN_PLC ³ CP_476 ³ SRC ³ 4 ³ ³
³ 44 ³ can_open ³ MAIN_PLC ³ CP_476 ³ SRC ³ 4 ³ SRC ³
³ 45 ³ can_slav ³ MAIN_PLC ³ CP_476 ³ SRC ³ 4 ³ SRC ³
³ 46 ³ pmc_plau ³ MAIN_PLC ³ CP_476 ³ SRC ³ 4 ³ SRC ³
³ 47 ³ printer ³ MAIN_PLC ³ CP_476 ³ SRC ³ 4 ³ SRC ³

  n.d : Task nicht in der Datenbank eingetragen



Hello,

both mentioned versions did not exist.

There was an Automation Studio 2.0 or 2.1 (no 2.01) and 2.38 did never exist

Are you sure that you need Automation Studio and not Automation runtime ? AR 2.01 and also 2.38 would exist

If the project you own has a “.GDM” file then you couls open this with any text editor and it would show the used AS version

From this on we could investigate further which AS and AR you would need

best regards

Oliver

You will most likely need PG2000, which is a very old programming system that runs under DOS.

PG2000 installation (request for sw) - Ask Questions / B&R Software & Runtime - B&R Community

Thank you for your reply.

I have got 2 diskettes but not run in dos or win95 &winxp

Is it possible send to us pg2000 program/on my email:sharif110@gmail.com

best regard-ghassem sharif

Thanks a lot for your fast reply

I willl send you a private message containing PG2000

best regards

Oliver

Dear Mr Oliver Doberer

Thank you for your attention and support

At the moment I am using pg2000 ver 2.44

Whit a co476 os v2.27

I would like reprogram plc but I think the os program on plc was damaged and I must be at first reload os on cp476

Is there any file about this matter?

After that this matter run by pg2000 or another program?

Hello @anon7194701

I am sorry to tell but my PG2000 experience is almost 25 years ago and therefor I cannot help here

best regards

Oliver

Very well thank you :folded_hands:

Good day, I have B&R 2003 legacy plc , may you please send me PG2000 software or old version Automation studio in the following email address

thembalucasmbatha@gmail.com

thembalucasmbatha@gmail.com

Hello @Themba

I can send you PG2000 but older versions of Automation Studio must not be sent by the community

Please see this post here:

How to Obtain Older Versions of Automation Studio [ AS2 | AS2.7 | AS3.0 | AS4.x ] - Share Info & Ideas / How-To & Wikis - B&R Community

best regards

Oliver