Hello and happy new year 
I want to use the different CPU cores for cyclic task classes as mentioned here: RELEASE 2025: Automation Studio 6.5 - Complete overview
I created a new AS Project to test it (AS6.5.0.306, AR6.5) but the “CPU Core” setting is not visible. I tested APC3200/APC3100/X20CP1686X and enabled advanced parameters but I still can not see it. Do I need to add something extra first to see this setting?
Greetings Jonas
I just tested this with new AS6.5 project and for me I the selection is available there, even without enabling advanced parameter visibility.
Are you sure your project is using AR6.5?
Hello,
as i did the test also at same time, here my pictures. I came to same conclusion. Please verify the used AR-Version via Change Runtime.
Greetings
Michael
Hi,
from what I’ve checked you also need the newest version of HW_Upgrade for the given device. I’ve checked with 5APC3200_RPL0_000 and for hardware upgrade 1.2.0.0 the task class core selection is available but for 1.1.0.0 it’s not.
Hello
Thank you for your inputs. I had not for all tested PC’s the newest version installed. With the newest update for APC3200 it is working now.
Greetings Jonas