Collision of shuttles in front of barrier

We have an ACOPOStrak with two connected ovals. At startup I send all shuttles to the smaller oval with MC_BR_RoutedMoveVel_AcpTrak. Then I MC_BR_BarrierCommand_AcpTrak to line up all the shuttles in front of a barrier. With one shuttle everything works as I expected. When I add more than one shuttle, the simulation with scene viewer works smoothly as well, but on the real system, the shuttles collide at the barrier.

According to my understanding MC_BR_RoutedMoveVel_AcpTrak generate elastic movements and I should not experience collisions. What do I need to do, to avoid collisions?

At every movement type the collision avoidance should do its work. With elastic you avoid errors when a shuttle is stopped by the barrier or other shuttle

Thank you very much for the heads up. After increasing the length the collisions do not occur anymore. The shuttle type was correct, however.