We are only working with one segment, that’s why we are only using one cable on the PCIe card
I think that’s probably your issue. SuperTrak requires both the Left and Right networks to be connected, meaning that the smallest possible configuration is a loop with two straight segments and two curved segments. As far as I know, there is no way to use a single segment of a SuperTrak.
At the very least, you need to be able to connect with Trakmaster to configure your layout. If you are unable to do this, there is probably an issue with how the SuperTrak library is configured in your project, the PCIe card is not correctly added to the Physical View, or there is a network error between your development PC and the SuperTrak controller PC.
Hello, we already got the connection with TrakMaster!, I share with you the errors that appear, the demo has only one segment but before it worked normally, it is the same project, we have not modified it.
The demo was only left unused for about 3 months. We have not modified connections or the project.
Sorry for the incorrect information, Alejandro! I had previously thought this wasn’t possible, but now I see that you can in fact configure a linear system in the System Layout.
From your last screenshot, it looks to me that the software is not physically communicating with the segment. There are communication errors, but I also don’t see the segment in your list. For reference, this is what my (simulated) Trakmaster interface looks like:
As you can see, there is a section 1 in the list, whereas in your screenshot, there are no sections. Since I haven’t worked with a linear layout before I may be missing something, but this is what I would troubleshoot in your case:
Check the System Layout in Trakmaster. Can you please share a screenshot of this?
The first picture in your first post shows the gateway network (Ethernet) cable plugged into the right side of the segment, meaning it is on the Right network. However, it looks like your cable is plugged into the Left network port of the SuperTrak PC card. Try swapping one of these, and make sure it matches your System Layout. If your segment is on the Left network in Trakmaster, both sides of the Ethernet cable should be plugged into the Left network side of their respective interfaces.