Does ACOPOS P3 support motors with EnDat encoders and motors with resolvers

Does P3 Dual drive support endat motors with resolver motor?

Hi,
this makes no sense:

If your questions is: Does ACOPOS P3 support motors with EnDat encoders and motors with resolvers, the answer is:

  • The on-board interfaces only support digital encoders (EnDat, Biss, SSI…), not resolvers
  • Resolvers can be connected to a plug-in card 8EAC0122.001-x or 8EAC0122.003-x

Sir, in P3 drive configuration what encoder interface type should select for resolver motor ?
We are using 8EI8X8 Drive and 8LSA44DB0.. and 8LSA55R20..motor also plug in module- 8EAC0122.003-1.

When using mapp Motion, in the configuration of the 8EAC0122.003-1 only “Resolver” can be selected.

In the configuration of the P3 drive, select “Not used” for the on-board encoder interfaces and under “Encoder link” for your axis select the interface on the plug-in card.