Error : Can not create directory during ArSim start up

simülation çalıştırmak istediğimde aşağıdaki hatayı alıyorum nedeni nedir yardımcı olurmusunuz ?

13 Error 24.10.2024 21:37:17,6658 \LOG APPLICATIONSTORAGEWRITER_PREPAREMODULECONTENDIRECTORY_CANNOT_CREATE_DIRECTORY:

I would say close Automation studio, delete temp folder in your project folder,move your project to folder C:\Temp, start Automation Studio as a admin, open project, rebuild all and execute offline transfer.

It would be helpful if you shared a screenshot of your error with us

The error counter does not exist is self explaining. Program is not downloaded in PLC. I created this step by step guide Getting started with B&R, "Hello community" first project, backend "PLC" part. Maybe try this first.

can you update me,anything new?

Hello, I couldn’t understand your answer. I want to run in simulation mode without a real PLC to test my program, but I get the error I shared with you. Could you please provide more details?

Merhaba,
Bilgisayarınızın tarih/saat formatından kaynaklı bu hatayı alıyorsunuz. Bölgesel tarih/saat formatınızı resimdeki gibi değiştirin ve projenizi tekrar derleyin.

Hi,
You are getting this error due to your PC’s date/time format. Change your regional date/time format as shown in the screenshot and rebuild your project.

I tried this, it didn’t work

How big is your project? can you save it as a zip file without upgrades and share it here? I would like to test it. Could be that problem is related to your laptop or installation of Automation studio.

Uploading: Screenshot_11.png…
I am currently getting the following error with error 444.
C:\BrAutomation\new_1\Physical\Config1\X20CP1685\mappView\Visualizat.vis (Ln:2, Col:2) : Error : ERROR: Start page is wrong or missing!

But this is something else. This is error from mappView, you have configuration file but you have not configured starting page for mappView. So check if starting page is existing, configured in the *.vis file. Could be that you renamed it?

Merhaba, gönderdiğiniz screenshotlar’da ilk bakışta yeni bir projeyle çalışıyormuşsunuz gibi gözüküyor. Yeni projeler normal şartlarda mappView paketleri içermez. Bunu siz eklemişsiniz ancak yapılandırmaya devam etmemişsiniz gibi duruyor. ConfigurationView sekmesindeki MappView klasörünün içerisinde .vis uzantılı bir dosya olması gerekiyor. Jaroslav’ın da bahsettiği üzere bu dosyanın içerisindeki start sayfası bulunamıyor. mappView kullanmayacaksanız .vis dosyasını silmenizi öneririm. mappView kullanmak istemeniz durumunda start sayfasını yapılandırmanız gerekiyor. Ancak bu konunun simülasyon modunun açılmaması ile alakası bulunmuyor.

Hello, in the screenshots you sent, it looks like you are working with a new project at first glance. New projects do not normally include mappView packages. It looks like you added it but did not continue the configuration of this service. There should be a file with a .vis extension in the MappView folder in the ConfigurationView tab. As Jaroslav mentioned, the start page in this file cannot be found. If you are not going to use mappView, I recommend you to delete the .vis file. If you want to use mappView, you need to configure the start page. However, this issue has nothing to do with the simulation mode not performing.

thanks. I solved the problems, changed the timezone, then put a / instead of a period between the date and it was solved. When I install the display software, operation does not start. What is the reason for this?

Uploading: Screenshot_3.png…
Bu şekilde kalıyor.

Sorununuzun çözüldüğüne sevindim. Göndermiş olduğunuz resimde problem olduğu için görüntüleyemiyorum. Başka bir konu hakkında desteğe ihtiyacınız var ise bu konuyla alakalı olmayan başka bir başlık üzerinden destek talep edebilirsiniz.

I’m happy your problem was solved. I can’t see the image you sent because there is a problem. If you need support on another issue, you can always create different topics about it.