Error Code when opening SAFEDESIGNER

This comes up, after im trying to open the SafeDESIGNER from my X20SLX806

Hello Yannic,

the error may indicate that a hardware file is missing in the project.

Hello,

If you open the SLX configuration (a right click), is the SafeDESIGNER version chosen?

Hello,
i opened AS and Rebuild his Hardware Tree. I got the error too… casue not clear jet.
So it is not only on his PC.

Greetings
Michael

Hello,
next Update, i have now a not working Version and a working Version.
Difference was that i set up Safety Release before inserting the SLX806.

  • Did you switched from MappSafety to SafetyRelease in your Project after inserting SLX?

Greetings
Michael

Hello,

@pavel.vavra
you are right. it was the missing SafeDesigner Version selection.
I thought i have checked it, but after closeing and reopening it was definitly empty.

Be also aware that the right SLX-Harware version is selected.
you need some 1.10.xx Version.

I may also add that if changing from MappSafety you have to manualy adapt the Libraries.
Remove:
* SfDomain
* MpBase ( only if no other Mapp-Component is used)

Add:
* AsSafety
* AsXml
* DataObj
* FileIO
* standard

Greetings
Michael

Hi @yaree98, I think you got a lot of good advice here. Is your issue solved?