Facing problem in Installation of APROL R4.2 (SLES 12 SP3) in 13th Generation Del CPU

I am facing problem in installing APROL R4.2-07 (SLES 12 SP3) in 13th Gen Intel Core i5-13600 DEL CPU.

While installing AutoYast I am getting stucked at
“Loading Ram Disk” I have uploaded refence image in attachment.

I have to install R4.2 in this CPU. So how can i proceed with this.

CPU Detail:
OptiPlex Tower 7010
13th Gen Intel Core i5-13600 ( 14 Cores/24MB/20T/2.7GHz to 5.0GHz/65W)

  • Windows 11 Pro, English
  • 32GB (2x16GB) DDR4 Non-ECC Memory
  • NAMD Radeon RX 6300 2GB GDDR6,Full Height,2xDP
  • M.2 2230 256GB PCIe NVMe Class 35 Solid State Drive
  • Additional 2.5 inch 1TB 7200rpm Hard Disk Drive
  • Intel Rapid Storage Technology, OptiPlex Tower

Auto Yast Source File used for instalation of AutoYast:
APROL-AutoYaST-DVD-V4.2-070.0.231002-SLE12-SP3

I dont have the Answer to your Question, but i can tell you that i had simmilar Problems with R4.2-06.

I have tried to Install it on a i5 12th Gen CPU and failed, i did made it thru the Setup process but the OS behaved in strange Ways.
I then tried R4.4 an it worked flawless at first Try.

Keep in Mind that Aprol R4.2-07 is bases on SLES12 wich was released all the Way back in 2017.
I dont think that the Support for Intel Power and Efficiency Cores was implemented at that Time.

This was already a topic with you in a Teams channel
Here the Statements:
1: from Christian Peham:
In my opinion, you will not have success to install the old SLES13 SP3, which is already more than 10 years old on the new hardware.
I guess this AutoYast, which you like to use, doesn’t content the device drivers for your new server hardware.

I recommend to use a standar B&R APC or certificied hardware from our homepage.

https://www.br-automation.com/en/products/process-control/aprol-hardware/

Another option, and in my opinion the best, is to install R4.4 with the new OS SLES15 SP4

  1. From myself:
    Who told you that this Hardware will work? This is not tested and evaluated from B&R.

See link from Christian.

→ possible solutions:

  1. APROL R4.4-xx (I recommend the latest one with the latest patch)

  2. Virtualisation (e.g: ESXi)