HMI Response Lag on B&R 4PPC50.101E-10A – How Can I Improve Performance?

,

Hello B&R Community,

I am experiencing a slight lag when pressing buttons on the HMI of my B&R 4PPC50.101E-10A Panel PC. When I click a button, the response is not as immediate as expected.

Previously, a boot animation was enabled, but I have disabled it to check whether it was affecting the HMI performance. However, the issue still persists.

I have also made the following changes in Automation Studio 4.12:

Disabled the boot animation.

Changed the VNC server refresh rate to 100 ms.

Changed the system timer interface to EPL/X2X Interface.

Despite these changes, I am still experiencing a noticeable delay when interacting with the HMI.

My questions are:

What could be causing this delay when pressing HMI buttons?

Are there any recommended settings in Automation Studio 4.12 to improve HMI responsiveness?

Could the issue be related to the VNC configuration, system timer settings, visualization update cycle, or PLC task cycle time?

Are there any other configuration changes or troubleshooting steps I should try?

I have attached a screenshot of my current configuration for reference.

Any suggestions or guidance would be greatly appreciated.

Thank you!

C50 is actually T50+CP0484, if I’m not mistaken. So you can also look for tips on VC4 and T50. There are some discussions here about it. It’s also a question of what realistic expectations you have for the response time of your VC4 visualization, which runs on the VNC Server and is accessed via a VNC client. Therefore, as a first step, I would create a new, empty test visualization, add your button and the function that triggers it, or perhaps just navigation. Since it will be an empty visualization without layers and images, you’ll get an idea of the best possible response time. Then you can see how far your current response time is from this best possible scenario.