How can load OS to 4PPC70 plc , if I can not put The plc in BOOT mode. I reset the plc and nor can not load OS start the PLC but never load the OS

I reset one PLC $PPC70 from the reset button, and now never start, not load OS, ans can not put in BOOT mode and can not connet with As software.

and not read the USB becase never put in BOOt mode.

Hello and welcome to the Community,

From my experience, if there is no HW fault, it should always be possible to switch to the BOOT mode with the reset button. Are you doing it properly - press the key briefly, a short pause, and then press and hold the key? It can sometimes be a bit tricky.

Hi @Hugo_Guerrero , what is the status of your topic, have you been able to load OS to your PPC70?

No I can not load because never put the ip adress in the plc

I never put in BOOT i do all the combinations possible with the reset bottom

Is it new hw or used one?

Used one, I was used in one machine but disarm it.

the PLC was work only reset with button.