Hi,
Automation Runtimes are not only installed per-version but also per-target. It looks like you maybe have installed the I3.10 version for your X20CP1485-1 but didn’t install it for the PP100 target.
https://www.br-automation.com/en/downloads/software/automation-runtime/automation-studio-3090/v30-ar-upgrade-i0310-pp100/
Maybe installing this will solve it.
Best regards
I don’t understand your question. In your “change runtime” dialog I can see a V3.08 being installed - which should be working and would be considered a downgrade. Why would you need to downgrade, though?
Sorry for my vague language. I’ll try my best to be clear.
It is an old project. PLC runtime is D3.07. Now it works on PLC pretty well. But we lost our CF for panel. I want to make compact flash for MP181 panel from source code. Project compiles without errors. However, when I make compact flash, panel can’t boot (you can see in picture). I think it’s because of different versions of PLC and AR panel which are installed on my PC. Maybe I should find an older version of the software to fix all this.