1. Make sure that the right mapp Motion version is on your PLC/APC (mappMotion V6.4.1)
2. Configure your system and cabling for single use of a 180 compact segment
3. Disable Power Supply of the segment
4. Disconnect PLK connection of the segment
5. Plug in Display (should not be powered on because of segment powered off)
6. Press and hold button1 and button4 of the display
7. Power on the segment (no PLK connection)
8. “connecting..” appears on the display
9. Release buttons on the display
10. “connecting…” and then “loading firmware” appears on the display
11. “BSL NN[node]” should appear
12. Connect PLK to running PLC/APC (FW should be downloaded and a restart should be carried out)
13. After reboot, the display should now show the correct version “6.3.*”