I’m using the PPC50 for my application and I need both USB interfaces for my automation runtime. So USB IF4, which is per default connected to the terminal, is reconfigured to connect to AR.
Now the technicians need to update the terminal OS on the machines in the field. How can it be done when the USB is not connected anymore to the terminal?
In the category “Update” of the terminal configuration settings of the C50, I can select the mode between “User-defined update server” and specify a server URL or the mode “Application”. Since the machine is not connected to any network, the first option is not applicable. Can we use the option “Application” for that? I couldn’t find any further documentation about that.
In the documentation we can see, that it is available from version 1.8.0 from april this year. So if you have an older version on your C50, it will not work, because of the installed version has not this feature. So I think you need to update it first manually via USB-stick and than later in the future it is possible to update to newer versions via AR.
You can download the C50 Linux images into Automation Studio via Tools-Upgrades:
I’m also unsure about the application trigger.
But just to mention it: the update server for the terminal os could also be the PLC integrated AR web or ftp server, at least I think so.
I have a C50 sample with terminal OS V1.3.1 installed and tried to update the terminal OS from its own FTP server to the latest V1.8.0 (as FTP is already enabled there). I have to mention that the C50 server is using FTPS (not unsecure FTP) with port 21 configured.
The steps I did:
Connect via Filezilla to the C50, create a folder “Update” and upload the terminal OS update files to this folder (unzipped - as I would do when using the USB update method)
In AS under the section “Terminal configuration/Update”, enter the URL to the update files