Ladder issues MpAxisBasic FuB

Hello everyone,

I’m having a problem with the ladder editor. When I try to insert a motion block and assign its outputs to coils, the interface won’t let me. It forces me to use an analogue output… I’m using AS 6.5.2.12

Have you ever encountered this problem?
Do you have a solution?

Kind regards,

Hi there,

I just tried it myself. Once I remove the “ENO” output line, it works - but then you can’t connect the ENO line anymore. It looks like this is expected behavior though, if I understand the help correctly - see “Default mode” here

  • Additional Boolean outputs are not permitted to be connected further. Only analog values can be connected to these.

I switched it to legacy mode - it lets me insert coils after that

Hope that helps

Edit: “Analog” value could be misleading - you can also attach a boolean value there! So if you don’t insist on a coil, just use that

Hi @Clement_Auffret, Michael provided you some suggestions, have you solved it?

Thanks a lot :folded_hands: that solve my problem.

Thanks for your faster answer :wink: