Hello everyone,
we’re working alot with the B&R-Library “Burklimat NG”. Now using this library requires a license. I am aware that my company is aquiring those licenses, but im not sure on how to properly install them. When doing a build or rebuild of a project which uses this library, i get a warning that one or more used components require licensing. Also when downloading the project to a PLC, it shows a yellow triangle next to “Run” in the status bar of Automation Studio, the logger has an entry about missing license, as well as the PLC’s “r/e” LED is blinking red.
My colleague claims that we just need to install a special module (X20 CMR100) and i noticed that we have 2 different types of them. One plain, and one with a sticker with a barcode that says something about “Technology guard configuration” and some number.
So my questions are:
- How does one properly install the license on a CPU
- whats this about with the different modules? Do those with the sticker contain a license, and those without a sticker don’t?
Any clarification on this is greatly appreciated!