MappView stop communicate OPC UA

I have problem with mappView after some last changes. But I don’t know why/where. After some time (few hours?) the panel, Web browser on PC,… sto communicate. There is only some xx values. But the Visu it’s loaded/reloaded. In log I see some OPC logout info and after this some errors with communications. Do you have some idea, what’s wrong?

The CPU usage go cca from 40% to 100% after this :exploding_head:

I first saw after update from 6.1.1 to 6.2.0 (AR, mappView, mappServices). I try to go back, but the problem is still here :roll_eyes:

I also find this https://community.br-automation.com/t/as6-1-opc-ua-communication-problem/6333, but if I remember, I have another probems in AR6.0.x and AR 6.3.x I dont see to download.

Helle @NovotnyJ ,
the reference post seems to be the solution. Either AR 6.0 which is available or AR 6.3 which should be available next week, since it releases 1st of June.

BR Fabian

Hi @NovotnyJ, I marked @fabian.pries answer as a solution for your issue. Feel free to update us if there is any new/different findings, thanks :wink: