Need to download B&R Automation studio v 2.6.0.14 sp04

Dears
I need help to download B&R Automation studio 2.6.0.14 sp04

Hi @bahgatismail have you tried to download that from our website?

Ciao
Valerio

HI
I have tried but i need the full AS first

I was worried about that.
I need to ask our local Support next step.

Ciao
Valerio

Hello,

Consider using AS 2.7 if it’s possible. Check this topic for details.

Hi,
Can you please send me a download link : bahgat@gmx.at

I just would like to mention that the licence servers for AS versions below AS2.7 no longer exist

This means that such old versions can only be used if an “old” licence already key exists.

Otherwise an activation of the software is no longer possible and you have to use AS2.7 which comes without any licence fee (and therefor also no need for a licence key)

Fully agree with @oliver_D. What is more, the change from AS2.6 to AS2.7 is not very dramatic, so it should not cause any big issue. But for sure, you have to update your project. Maybe you can tell us for what exactly you need AS2.6 (SW changes and download or online monitoring only?), maybe we will help you find an easy way how to solve your issue.

Dear Mr.Jaroslav,
I need it for a machine that is running with this version(2.6.0.14) and i need to upload the Program so i can monitor the machine program

Do you have project? You can not upload source files from PLC.

@bahgatismail during my first training in Eggelsberg I used AS 2.6, in that moment mapp Technology was not ready yet, same story for safety, ACOPOStrak, Supertrak,vision system.
In that moment in AS prj was only important the AR version, VC4 firmware version and most important ACP10 version (I’m positive your machine is not running cnc so you don’t need ARNC0 too).
If you have installed AS 2.7 you can connect to the machine where the prj was developed with AS 2.6 and you can:

  1. upload the system logger (SDM is not developed yet on the runtime installed on your machine)
  2. trace variables
  3. Upload network command trace

so you have all tools for troubleshooting the issue (for sure there is an issue otherwise you are not here).
Ciao
Valerio