Need to download B&R Automation studio v 2.6.0.14 sp04

@bahgatismail during my first training in Eggelsberg I used AS 2.6, in that moment mapp Technology was not ready yet, same story for safety, ACOPOStrak, Supertrak,vision system.
In that moment in AS prj was only important the AR version, VC4 firmware version and most important ACP10 version (I’m positive your machine is not running cnc so you don’t need ARNC0 too).
If you have installed AS 2.7 you can connect to the machine where the prj was developed with AS 2.6 and you can:

  1. upload the system logger (SDM is not developed yet on the runtime installed on your machine)
  2. trace variables
  3. Upload network command trace

so you have all tools for troubleshooting the issue (for sure there is an issue otherwise you are not here).
Ciao
Valerio

1 Like