Not able to add Mapp Technology MpAxis Basic in a program

I have an issue in adding the Mapp Technology Package MpAxisBasic in a program , I tried to search in the search box as well
its not visible.

In Change Runtime version ,It is visible as Mapp Services but i have an another Project
in which it is named as mapp, in that project MpAxisBasic is available , so how can i do it in this project??

Below is the image in which MpAxis basic is available and it is named as Mapp , If It’s Only available in Mapp then how to add it?

Thank you for your assistance

Regards
Sundeep

Hello,

your second project made use of Mapp Legacy which is based on older versions of ACP10

and which is obsolete now.

Current versions of ACP10 can not use Mapp Legacy.

From my point of view he most promising approach is to build the project on Mapp Motion.

Your version dialog then will look different:

Starting with version 5.x, the mapp Motion package must be installed to use MpAxisBasic. Earlier versions of mapp 1.x handled this differently. Caution is advised, as there are minor differences in usage.

If you are using ACP10 and not mapp Motion, the mpAxisBasic configuration files are added in the Motion folder, not to the Services folder.

Yes but how to enable motion folder ?? i am not able to add it

Hello,

The Motion folder appears automatically if you choose the ACP10 ARNC0 version.

MotionFolder

Also if you add a drive it will whether you want to use ACP10 or mapp Motion. Then there will be a motion folder.

Its Working !! Thank you