Save/Load McAcpAxRestorePosType from XML File

In the past i felt secure enough that McAcpAxRestorePosType would not get lost when i was able to use .per files. However now that those arent supported i want to be able to export my restorehomeposition variables to an xml file for backup, and then later to be able to restore them if needed. When going through the help i ran across this bit of information that restore position cant be written to via the application.

Is there another function im not aware of that can be used to backup and load variables of the McAcpAxRestorePosType type?

Store cyclically data to USB mass storage - Ask Questions / B&R Software & Runtime - B&R Community

This has been discussed before and I don’t recall having seen a good solution.