Hello All
I have Trouble with Panel Firmware Version 1.7.0 with Cyber security Features added to the project My Observations : Panel gets Stuck or to say freeze in a page for long time after a refresh it starts to work . Another test was made without Cyber security features added to the project its seems to work fine .
In parallel i have another panel where i have installed the panel with firmware version V1.6.0 It seems to run without any problem , i am running with the same project with cyber security features added.
Does anyone have the same problem with Panel Firmware version V1.7.0
Hi Arun,
Which features/settings are you referring to when you say “Cyber security Features”? Does version 1.7.0 work for you without these features enabled?
Also, please remember that the Community is not the place to report bugs! If you believe your issues stem from a particular firmware version (rather than your application/settings) then we will not be able to help you, and I instead recommend you reach out to your local B&R office/Support team.
Thank you for the response , I didn’t Frame the Question Properly my mistake , i can explain in a better way .I am attaching the images for the Cyber features i am currently using.
I have issue with below given test case :
Test Setup1: T80Panel with Firmware V 1.7.0 and Cyber Features Added Project (HTTPS,SSLConfigurationOPCUA Encryption)Please Refer to attached image.
Using automation studio V4.12.6.106 Created CF card for the project ,Inserted CF Card in X20Cp1586
TEST CASE 1: Logged in the Panel then Logged Out the Panel , Removed the Power Supply for the panel , Again Connected the Power Supply for the Panel Logged In but cannot logout , Panel Got stuck in the same page .
TestSetup 2 : T80Panel with Firmware V 1.6.0 and Cyber Features Added Project (HTTPS,SSLConfigurationOPCUA Encryption)Please Refer to attached image.
Using automation studio V4.12.6.106 Created CF card for the project ,Inserted CF Card in X20Cp1586
Test Case : I did the same test case as mentioned in the previous TEST CASE 1 , the panel was running without Problems
Test Setup 3: T80 Panel with Firmware V 1.7.0 , Project without cyber features added to the project
Using automation studio V4.12.6.106 Created CF card for the project ,Inserted CF Card in X20Cp1586
Test Case : I did the same test case as mentioned in the previous TEST CASE 1 , the panel was running without Problems
Find the attachment for the images :
Thank you .
Thanks for the detailed information! Unfortunately, I don’t have any ideas, and it doesn’t look like the Community does either. This may be a bug and so I recommend you reach out to your local B&R support team as we cannot help you with those here.