I’m experiencing an issue with running the visualization on the Panel (model 5AP1120.1505) connected to an APC4100. The APC is in “Run” mode, but the visualization does not start. compiled with AS6.3.4
The VNC configuration on the ethernet interface is used for access to vc4 thought ethernet. I tried to replicate the your situation, and only managed to do it, if the there are other ethernet interface already using this vc4 object. Maybe you can check the status form other IF.
The problem only exists on APC4100 with SDL4, i have another configuration with APC910, with SDL3 interface and there all is running fine. On the configuration side of ETH2 is nothing connected
Thank you very much for your support on this topic.
I also contacted B&R support, and they confirmed that with the new APC4100, VC4 visualization is no longer supported due to the Cyber Resilience Act. With firmware version 1.0.0.0, it was still possible to reference a VC4 visualization to a panel. However, starting from version 1.2.0.0, this option is no longer available, and this behavior is intentional.
Alternatively, using a Windows 10 operating system is still a viable option, as VC4 visualization can work in that environment.