View Camera Live Stream in HMI

Hello everyone,

we are currently trying to find a solution to display a camera live feed on an HMI.
The following two topics are already known to me:

and

In the past, we used standard IP surveillance cameras, adjusted their configuration, and were able to access the camera’s MJPEG stream directly in the MappView visualization via a browser.

Over the last years, we have observed that several camera manufacturers have changed this behavior. Camera models or revisions that previously supported unauthenticated browser-based live streams removed this functionality in newer revisions or updates.

While this change is not explicitly mandated by the Cyber Resilience Act (CRA), it appears to be related to the general shift towards “security by default” and stricter access control requirements. As a result, browser-based live images without authentication or verification are becoming increasingly harder to use in practice.

Authentication via the URL in the form username:password@ip-address still works with some manufacturers. However, this approach will disappear in the long term, as credentials are transmitted unencrypted. In addition, the browser integrated into MappView does not support this type of authentication anymore or possibly never did.

Our requirement for the camera system is that it should remain simple:

A camera provides the image → the MappView client (or server) accesses it directly.
No intermediate components.

We are aware of various solutions involving ffmpeg, VLC, and plugins. However, we are looking for (and have been asking whether it could be considered by B&R for quite some time) a native solution. Ideally, this solution should also work smoothly in spare-part scenarios and should not require any client-side modifications on the MappView HMI.

Solutions based on installed certificates have not been convincing for us so far. Certificates of the camera are often only valid for a few years and after that lifespan require updates before the camera image can be displayed again. From our perspective, this is not an industrial-grade solution in terms of lifecycle, maintenance effort, and long-term availability.

We are aware that displaying a camera live feed is not part of the standard feature set of an HMI. However, customers are very willing to buy this functionality. Many of them appreciate the convenience of having everything integrated into a single HMI instead of operating multiple screens on a machine.

My questions:

  • What is B&R’s position on this topic? Are there any efforts to improve the compatibility of MappView with video streams, authentication mechanisms, and camera systems?
  • Can the experience within this forum help here? Are there ideas or implementations we may not have considered yet?
  • Are there camera manufacturers that support exactly this kind of simple, direct integration and are likely to continue supporting it in the future?

Thank you very much for any hints and for brainstorming together :slight_smile:

Hi @Bjorn_Kanter ,
thanks for your post, it’s very interesting topic.
I recommend in your case to contact your local B&R office, have a meeting with our engineering manager or director of engineering and the Sales responsible for your area.
I’m sure after that, colleagues will send your requests to R&D and give you an answer.
In most of the countries we have a vision expert, in US we have one and He is normally involved in the more complex vision applications or on proof of concept, I’m sure we have one
in your area too.
Thanks
Ciao
Valerio

Hi @valerio.manenti,
thanks for your answer. We already did a while ago.
I still have hope that there are some good Ideas in the community but to make the problem better understandable I have written this detailed explanation.

Hi Björn,

Your post highlights a challenge I’ve also faced: integrating a live IP camera feed directly into MappView without relying on complex third-party solutions or camera-specific features. Here’s what worked for me and some ideas that might help you or others in the community:

1. Centralized Recorder (NVR) Solution

I ended up using a Network Video Recorder (NVR) to centralize camera feeds. The NVR provides:

  • Direct HTTP-based live streaming, compatible with MappView’s built-in browser, I was able to create a unique URL with authentication token.
  • Centralized authentication and certificate management, simplifying long-term maintenance.

Pros:

  • Independent of individual camera features.
  • Easier to manage security updates (certificates, authentication).
  • More robust for industrial environments (lifecycle, maintenance).

Cons:

  • Adds an extra hardware/software component, but it’s transparent for end-users.

2. Custom Widget with WDTC

You mentioned a native B&R solution. A custom widget using WDTC could be a way forward.

3. Cameras with Simple Stream Support

Some manufacturers still offer cameras with simple MJPEG or HLS streams. Consider:

  • Axis Communications: Some models support MJPEG with configurable security.
  • Mobotix: Known for industrial solutions with HTTP-accessible streams.
  • Hikvision (select models): Check for MJPEG support, but verify recent firmware updates.

4. Other Ideas

  • Local Proxy: Use a small server (e.g., Node.js + FFmpeg) to convert RTSP to HLS and serve it via HTTP. MappView accesses the proxy.
  • WebRTC: Some cameras support WebRTC, which can be integrated via a custom widget.

Hope this could help!

Regards,
Florent

Thanks a lot!
mobotix looks really interesting. We’ll get in contact with them :slight_smile: