VNC on Power Panel 4PPC50?

Hello, I have a question.
Is it possible to use VNC Viewer on a remote PC and view the application on the PP terminal at the same time?

I’m using a 4PPC50.156B-13B Power Panel, and I’d like to run the application on the panel while also viewing it remotely through VNC Viewer.
I tried this, but when the terminal is initialized, I can’t connect to it via VNC Viewer.
However, if I don’t initialize the terminal and connect via VNC Viewer, the connection is successful.

Hi,

depending on your Automation Studio Version this could be different, but in your ETH-Configuration in the Projekt (VNC Servers), you can set the “max. connections” Parameter to “2”.

By default there is only one connection allowed at a time.
It sounds like this could fix your issue.