4PPC70.0573-20B stuck in Boot mode: SERVICE after trying to transfer Program

Hello B&R Community

I am completely new to AS4 and B&R in general, but i have gotten my hands on a C70 Panel that i wanted to try programming something onto. I configured my hardware, which is the aforementioned C70 Panel, along with an X20 Row that includes 5xSM1446-1 modules and 5xZF0000 Modules. However, when transferring the program, i updated the AR runtime version from F4.45 to J4.93. It is now in Boot mode: SERVICE, and the old IP that i used to access it no longer allows me access to the Panel. Do any of you know what i should try to do from here to get my project working? Thanks in Advance.

I forgot to mention, but i have also tried to ping other IPs in the hopes of getting access to the Panel, such as:

192.168.1.10

192.168.1.1

192.168.0.1

But none of them give me any response back on the controller.

Hello Emil, and welcome to the B&R world!

To get connected, you’ll first need to know how the IP address was configured in Automation Studio. The settings in the project you transferred would have overwritten anything that was already there. To see this, go to your Physical View, right-click on the Ethernet port, and go to Configuration. Can you please tell us what you see here?

The default setting is for the controller to get its IP address from a DHCP server. If it is not connected to one, then you can change this to “Set IP Address Manually” and enter an IP address and subnet. I also recommend setting SNMP to Activated for now. This will allow you to browse for the controller via the Online→Settings Browse window in Automation Studio if you forget the IP address.

To diagnose the Service mode, there are a handful of helpful posts on the Community about how to collect diagnostic information, such as Service Mode - What is it and how to collect diagnostics - Share Info & Ideas / How-To & Wikis - B&R Community and PLC module stuck in “BOOT mode: Service” - unexpected reboot and connection issues - Ask Questions / B&R Software & Runtime - B&R Community. Please take a look at the Logger once you get connected and let us know what error messages you see.

Hello Marcus

This is what my Settings for ETH on the Panel looked like when i opened them now. It seems that it did get the IP from a DHCP Server. Do you know how i would then determine what the current ip Then would be? i should mention, that i am running this on my home internet for now.

I will also take a look at the resources for how to diagnose the Service mode tomorrow.

Thank you for your input and patience.

Hi @Emil_Andreasen ,
normally in your case I follow the guidelines described in this post:

Thanks
Ciao
Valerio

1 Like

It’s very helpful that PLC is on your home network. The article Valerio linked is a good option. However, you can also access the administrator settings of your home router/modem and probably find it’s IP address there (if you’re familiar with how to do that).

If you were in this spot and couldn’t find the IP address, you would have to assign a static IP in Automation Studio, rebuild the project, and then do an offline installation. Since the C70 has no removable memory, this is done via a USB stick. That is always an option if you aren’t able to find the assigned IP address.

Hi @Emil_Andreasen , what is the status of your issue, have you established connection?

Hello Jaroslav, sorry for not replying any earlier.

I have managed to solve the issue! i logged into my router and found the automatically assigned IP, and then connected to it. After that, i have set the IP in my project to match the Automatically assigned IP, and have added a rule in my Router to keep giving the same IP to the Power Panel.

Thanks to the links that Marcus showed me, i also managed to identify and solve the problem with my hardware configuration, making it now boot into RUN mode. Big Thanks to Marcus for the help he has provided!

3 Likes