I have elimd 8EI4X5HWT10. I want to check only 1 axis of this, I get an error, how can I get rid of the error?
Hi,
error diagnosis on a picture with static red LEDs is quite hard. I recommend doing the usual error diagnostics: AS Help, Logger, SDM, Network command trace.
Have a look at the AS Help and there on the chapter about the LEDs first - it might already show you whats wrong: B&R Online Help
BR
Edit/P.S.: Whatās āelimdā? Canāt figure that one out.
The PLK of the APpoces 3 servo driver is constantly lit in red. how can i solve this
You need to either use the ACOPOS P3 display to change the node number or activate and configure Dynamic Node Allocation (DNA) on the managing node (PLC).
When I enter plk configuration, there is only a manual or automatic change place for DNA changing, I cannot find where it is.
yes I did it here. can be done automatically. Do I need to make any other settings? because it still has plk problem
@eem.ferhat please avoid creating new topics for the same issue - since your LED problem is pretty much the same as yesterday, I merged the two topics. Please continue in this thread
(linking @tommi.piiparinen so you also find the topic again)
The axis1, axis2, axis3 lights of my servo driver are flashing green. I also made the settings. I connected only 1 servo to my 3 servos system. but it just flashes green and does not become permanent green. Where could I have missed something?
green blinking means:
ānot all conditions to switch on the axis are presentā
e.g. no enable input, no mains voltage, no encoder connected etc.
but since we are not sure whether your project is ok
Mpaxisbase - Error Unknown data type - Ask Questions - B&R Community
it difficult to answer your question.
The simplest answer would be: just switch the axis on by using MappCockpit to get a proper error message what is missing.
Hello @eem.ferhat ,
once more I would like to ask you to not create new topics when you are basically still just have one topic āsetting up the driveā properly.
I merged this one into the existing thread again
Quick note: Please, whenever you ask another question, try adding details. Your thread didnāt contain any info about the drive (right now P3 is the only 3 axis drive, but not everyone might know this?), what are THE settings supposed to be and basically anything but āblinks greenā.
cc @christoph.hilchenbac for you to find the thread again