Hi I have a general question regarding the key differences that mappMotion brings to the table which ACP10 is unable to. Do anyone has a list of new features that does not exist in ACP10 ?
Hello Samuel,
you need to ask the question the other way around: Which functions does Mapp Motion *not yet* support that ACP10 has long been capable of?
By now, Mapp Motion is sufficiently developed that you can implement all the features of ACP10 using Mapp Motion as well.
Regards
Stephan
Hello,
If you want to have a look in the new Features List, you may use the
Mapp Motion - Version Informations
The most differences are found in the areas of Robotics and Mechatronic Systems.
For Sinlge Axis there are not so much differences because rotating a Motor was also good developed for ACP10. But there are some Tweeks added to the Control-Loop as well, especialy for more Flexible Systems. We have now the Possibility to use a ACOPOS as a Vibration source for Transport Systems.
Today there is no way around MappMotion, because development of ACP10 mostly stopped.
Greetings
Michael
Hi Everyone,
Thanks for the input it is much clearer for me now.