For creating the SDC file, you have the SafeDomain_BR part available. If you perform the compilation on that place "SafeDomain_BR ", the SDC will be created.
Hi Petr,
It seems that it is now generated even after the SafeDomain_BR build, whereas in the previous versions, the RemoteConfiguration had to be built as well.
Is there any documentation describing these different build processes?
Thank you.
Hi Michal,
the previous versions were in prerelease mode and under development.
The current information provided in the help applies: Actions in instances
Hi Petr,
in my case, the safety is loaded via SpServer FBs, and I thought that the RemoteConfiguration needed to be built. If there aren’t differences between the containers built in RemoteConfiguration and SafeDomain_BR, that’s perfectly fine, but this is not clear even from the help documentation.