After startup, C80 enters the N/A mode

During normal operation, C80 suddenly restarted and after startup, C80 entered the N/A mode.
At this moment, AS is unable to connect with C80, and SDM is also unable to connect.

Only after performing a USB update on the C80 will it return to normal.

What are the possibilities for C80 to enter the N/A category?

Hello,

If you can not get Access to the Device with the Automation Studio its difficult to get a logger entry. So hard to tell what goes wrong. I just start Brainstorming …

  • I would start with checking the Versions of B&R Software in comparison to latest version.
  • Does the application use some File-Write functions FileIO-Library or similar? If yes can they be temporary disabled for testing.
  • If the Device does not reconnect after the restart it looks like some how the AR-Installation gets corrupt but this is only a assumption.
  • Is it the only device showing this issue / do you have other C80 for Comparision?
  • Can you install a Empty Dummy Project, does it show same issues?
  • How long is the intervall of the issue daylie / weekly … ?

Downloads for C80 (Bios / Linux Image / User-Manual)

Checking versions

Greetings
Michael

Hi!

Michael Bertsch is right with his comment to update to the latest versions.

We had the issue that Linux and Automation Runtime due to the paralel access to memory trigger a race condition in the hypervisor. If you use Automation Studio 4 this issue is fixed with Automation Runtime O4.93. If you use Automation Studio 6 this issue is fixed with Automation Runtime 6.4.

Best regards, Manuel

Hi,

Thanks for reply.

  • Does the application use some File-Write functions FileIO-Library or similar? If yes can they be temporary disabled for testing.

》I need to verify this point.

  • Is it the only device showing this issue / do you have other C80 for Comparision?

》This is not an isolated case. It has also occurred on other C80 models.

  • Can you install a Empty Dummy Project, does it show same issues?

》I updated a new program via USB, and then C80 was able to return to normal.

  • How long is the intervall of the issue daylie / weekly … ?

》This is quite random. It might take several months. However, the same procedure did not result in any abnormalities on the PPC2200.

Thank you for your information.

I will recommend customer upgrade AR